Hi,
I want to use the device SN74LVC1G07 as a level shifter.
In my application the device is powered with 1.8V and the output will be connected to 2.0V with a pullup resistor.
I want to level shift a GPIO which 1.8V logic. Unfortunately this signal will be first 3.3V logic until it switches down to 1.8V logic.
Since I'm powering the device with 1.8V, is it possible to allow input voltages up to 3.3V?
Where can I find this information in the datasheet respectively which parameter describes this condition?
Will there be forward current through an ESD diode?
I'm asking because usually in datasheets the max input voltages are defined e.g. Vcc+0.7 volts.
Many thanks
Adrian