This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV14A: Statistical distribution about propagation delay

Part Number: SN74LV14A

Hi team,

Could you give me comment on following customer request?

<Customer request>

Q1. Could you share statistical distribution (e.g. Gaussian or Uniform distribution) about tpd as following condition? Those distribution directly influences on gate control circuit in motor drive and they want to estimate such distribution in gate control circuit. 

VCC=5V±0.5V

1. tpd((From A(INPUT) to Y(OUTPUT), CL=15pF, TA=25°C)

    :5.1ns(TYP)~8.6ns(MAX)

2. tpd((From A(INPUT) to Y(OUTPUT), CL= 50pF, TA=25°C)

    :6.7ns(TYP)~10.6ns(MAX)

3. tpd((From A(INPUT) to Y(OUTPUT), CL=15pF, TA=–40°C to 85°C)

    :1ns(MIN)~10ns(MAX)

4. tpd((From A(INPUT) to Y(OUTPUT), CL=50pF, TA=–40°C to 85°C)

    :1ns(MIN)~12ns(MAX)

5. tpd((From A(INPUT) to Y(OUTPUT), CL=15pF, TA=–40°C to 125°C)

    :1ns(MIN)~11ns(MAX)

6. tpd((From A(INPUT) to Y(OUTPUT), CL=50pF, TA=–40°C to 125°C)

    :1ns(MIN)~13ns(MAX)

Best regards,

Takeshi Sasaki