Hi,
Can we use VCC=1.8V,
1A = 1.8V pull up
2B = 5V pull up
1Y= 3.3V pull up
2Y = 1.8V pull up
Will it function good ? or will it cause any internal leakage issue ??
Please suggest.
Thanks,
Vignesh.M
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can we use VCC=1.8V,
1A = 1.8V pull up
2B = 5V pull up
1Y= 3.3V pull up
2Y = 1.8V pull up
Will it function good ? or will it cause any internal leakage issue ??
Please suggest.
Thanks,
Vignesh.M
Hi Vignesh,
Yes this will work. Per the datasheet: "Inputs and Open-Drain Outputs Accept Voltages Up to 5.5 V".
Thanks!
Chad Crosby
Thanks Chad Crosby,
But having various voltages at each different pin does not cause any issue?
I think only IO levels will be very strict ( depends on the VCC voltage )
No other issue right..
Pls confirm..
Thanks.
Vignesh.M
Hi Vignesh,
Section 6.3 of the datasheet mentions that for a logic signal to be recognized as a logic HIGH, its minimum value must be 0.65 x VCC (for a VCC = 1.65V to 1.95V). Section 6.3 further goes on to say that input voltages are recommended to be between 0 & 5.5V.
So, in short, yes this configuration will work.
Thanks!
Chad Crosby
Different voltages are no problem. See [FAQ] Can the input voltage (Vi) to my logic device be higher than the supply voltage (Vcc)?