This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2T45: _

Part Number: SN74LVC2T45
Other Parts Discussed in Thread: SN74LVC2G04, SN74AHCT1G04, LSF0102

I am looking for a component to replace the functionality of these two components, level shifter sn74lvc2t45 and inverter sn74lvc2g04. Data sheets are attached.

 

Requirments:

Input Voltage range: 3V-3.6V

Output Voltage Range: 5V

Max Tpd: 6ns or Tplh+Tplh is < 12 ns

Dual channel or more is a plus.