Customer has FPGA w/1.8V I2C bus, needs to interface to a pair of 5V powered I2C slave devices, SCLK = 1 MHz.
Any issues using TXS0102 in this secenario? The pair of slaves obviously have different addresses and should not contend. Another thread on this topic mentioned this should be OK so long as loading is < 70 pF on the line.
This particular board is rather small, so not anticipating traces adding much capacitance.
Also, would like to rely on the built-in pull-up resistors in the device instead of placing additional I2C pull-ups. Is this OK as well? Seems like 10K would be fine to maintain the bus, and the edge-accelerators can keep the edges clean.
Seems like this will work fine, Please confirm.
Thanks, Best, Steve