Other Parts Discussed in Thread: SN74AXC8T245
Good Day,
I would like to use the SN74AVC8T245 to translate signals from 1.8 V to 3.3 V.
In this case the propagation delays (t_PLH and t_PHL) varies between 0.5 and 3.9 ns (from A to B).
The min and max of this delay is specified for T_A of -40 to 85 degrees.
What would the min and max be at a fixed temperature of 25 degrees?
Kind regards,
Francois