Hi Sir,
May I ask is there any input voltage requirement for SN74LVC08A to have Y pin output?
We using this SN74LVC08APWR IC for AND two PWM signal.
We found out that if the A/B input voltage about 2.4V, there will no Y output signal.
If we pull the A/B side voltage level to about 3V, there will have Y output signal.
From the SPEC, we are wondering why there are no output from Y pin, our voltage level at A/B side have meet the SPEC requirement which > 2V.
Below is the 3V waveform and 2.4V waveform and the schematic, FYI.
Could you please help to advice it?
Thank you
FAN8_PWM/FAN9_PWM voltage level is about 3V.
FAN10_PWM/FAN11_PWM voltage level is about 2.46V.