This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0102: about Level shifter TXS0102 for I2C signal

Part Number: TXS0102
Other Parts Discussed in Thread: SN74LVC2G66

Dear team,

I plan to use level shifter TXS0102 for I2C signal. The voltage domain of VCCA and VCCB are both 3.3V.

TXS0102 needs VCCB >=VCCA. But our design are both 3.3V for VCCA (CAM_3V3) and VCCB(V_IO_3V3).

Will the ripple (<100mV)on VCCA and VCCB cause any issue? Also V_IO_3V3 and CAM_3V3 are from different LDO and may different a little bit.

Could you help check below schematic is ok or not? 

Thank you.

Kane