Other Parts Discussed in Thread: TXS0102
Dear colleague,
Our customer wants to use realize 1.2V and 1.8V transition based on I2C.
But we find it in datasheet, we don't know which one is right.
Thanks a lot!
Best Regards,
Rock Su
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The high-level signal voltages are determined only by the pull-up resistors on the signals. The Vref_A/Vref_B voltages are independent from those.
Just connect Vref_A to 1.2 V, and the Vref_B resistor to 2.5/3.3/5 V.
Using the TXS0102 instead would save the five external resistors.