• TI Thinks Resolved

SN74LV1T34: SN74LV1T34

Prodigy 40 points

Replies: 2

Views: 25

Part Number: SN74LV1T34

Hi,

I want to use this component to detect a 5V or 3.3V voltage and provide this detection information to an 1.8V interface controller (a FPGA).

Is this component can be used like this if i set the VCC to 1.8V ?

Reading the datasheet indicates that the Inputs are 5V input tolerant.

If you can confirm (or not) the possibility 

Thanks.