Other Parts Discussed in Thread: SN74LVC2G17, SN74HCS125
Hi team,
My customer is using the SN74LVC2G07 now. Currently the input signal of the device is as the waveform below. Whether the waveform has risks? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
My customer is using the SN74LVC2G07 now. Currently the input signal of the device is as the waveform below. Whether the waveform has risks? Thanks.
That edge is certainly slower than 10 ns/V. See [FAQ] How does a slow or floating input affect a CMOS device? for the risks.
You should use buffers with Schmitt-trigger inputs (SN74LVC2G17 if you can use push/pull outputs, or SN74HCS125 with the inputs connected to the OE pins if the outputs are not pulled above 3.3 V, or SN74LVC2G17 in front of the SN74LVC2G07 otherwise).