• Resolved

LSF0101: Is there minimum current value for LSF0101's I/O?

Prodigy 160 points

Replies: 10

Views: 66

Part Number: LSF0101

Hello TI team,

When I read the datasheet of the LSF0101, it seems that the current flowing to the I/O should be of the mA level (there are example for choosing pull-up resistor for 15mA, 10mA or 3mA and the test conditions are presented with current from 10mA to 64mA).

I need to use this translator for SPI communication. However, in the MCU I'm using, the SPI communication port have pull-up/down resistor of about 13kOhms. That means that for 5V there would be a current of approximately 385µA flowing in the switch of the LSF0101.

Would it still be alright or is there a minimum current value that should be flowing in the LSF0101 to make it work properly?

Thanks for your help.

  • Hey Ben,

    There is no minimum current needed, just a maximum to avoid damage to the device. This isn't usually the recommended device for SPI so there may be a better solution for this particular application if you give me more details on the signal you are trying to translate. That isn't to say this device won't work, and if you wish to forward with using it, I recommend checking out these training videos. They are very helpful when using the LSF family.

    Check out our new AXC family of Voltage Translators! 

    Watch the Introduction to AXC Family to find out more about the family.

  • The LSF outputs open-drain signals, so the size of the pull-up resistors directly affects the speed of the rising edges. You need a high current only if you want to achieve high frequencies.

    SPI, by itself, uses push/pull signals, so the pull-up/down resistors are needed only to avoid floating signals when the devices are idle. In other words, these 13 kΩ resistors do not affect the speed.

    Do you need to translate up or down? Do you have a MISO signal?

  • Hello Dylan and Clemens,

    Thanks for your respective answers :-)

    I actually need to translate several kind of signals to and from the MCU: the standard SPI ones (MISO, MOSI, SCLK and /CS), but also two other signals : one sent and one received by the MCU.

    The MCU is 3vdc powered and the data shall be transferred to another IC via a cable. The point to translate the voltage level is too keep the integrity of the signals during their path in the cable (which could be at most 2 meter long).

    To resume :

    MCU (3V) <==> Translator (3V->5V) <== CABLE (at most 2m) ==> Translator (5V ->3V0) <==> IC (3V)


    Furthermore, the MCU shall control up to 8 IC the same way, that is to say 8 x 6 = 48 signal to send this way.

    @Dylan : For practical reason, I'd prefer use translators which can manage as much bit as possible.
    I also found the part SN74LVCH8T45 and/or SN74LVC2T45 (configured for one way or the other depending of the signal, as there are no two direction signals). What would you think of these?

    @Clemens : I may have been misled by the following presentation www.ti.com/.../LSF0101
    I think I have answered your question in my presentation above :-)

  • In reply to Benjamin Nordman:

    A 2m cable has quite a high capacitance, so you will need even more current to get fast rising edges. Are the MCU and ICs capable of driving that current?

    There is not really much difference between 3 V and 5 V, but using translators might make sense if you want to use the stronger output drivers of the LVC family.

    If you are really concerned about signal integrity, you should use a much higher voltage (as in RS-232) or differential signals (as in LVDS; check out the SN75LVDS387‌/‌SN75LVDS386‌).

  • In reply to Clemens Ladisch:

    Hello Clemens,

    Thanks again for your new post.
    Indeed, I didn't taken into account the capacitance of the cable. Do you know a simulator (e.g. in LTspice) that could help me check this matter?

    In any case, I'm sorry but even if your idea is a good one, I could not use the SN75LVDS387‌/‌SN75LVDS386.
    Indeed, I'm limited in number of wires to send the data and the connector I have to use is already full.

    If ever there is no other idea, I think I'll take my chance with the SN74LVCH8T45.

  • In reply to Benjamin Nordman:

    Hey Ben,

    Yes this is a very long cable for a translation device in our portfolio to drive, but your best bet will indeed be to use the SN74LVC8T245 and the SN74LVC2T45 devices. They will provide the strongest drive strength and may be able to drive the capacitance of the cable while maintaining good enough signal integrity at the other end. Can't really say for sure, but you can always use the IBIS model to simulate this. My biggest concern would be slower transition time causing some issues on the other end.

    Check out our new AXC family of Voltage Translators! 

    Watch the Introduction to AXC Family to find out more about the family.

  • In reply to Dylan Hubbard:

    Hello Dylan,

    Thank for your reply. I'll try to perform some simulations with the IBIS model.

    Just for my understanding, could you please tell me the difference between the SN74LVCH8T45 and the SN74LVC8T45?
    The electrical characteristics seems the same to me (same pinout, voltage/current maximum rating, operating temperature limit, consumption almost the same switching time characteristics).

  • In reply to Benjamin Nordman:

    Hello,

    The (H) in the part number indicates Bus-hold circuits added to all data inputs. There's an app note that explains these here:  


    Looking for a low voltage translator? Check out the AXC family that supports 0.7V to 3.3V translation!

    The Logic Minute training page has videos on many interesting topics that all are kept shorter than 5 minutes.

  • In reply to Emrys Maier:

    Hello Emrys,

    Thanks for the documentation :-)

  • In reply to Dylan Hubbard:

    Thanks again for your help :-)