Other Parts Discussed in Thread: TXS0108E
Hello TI Forum,
I am using the TXB0108 to shift the logic level of a microcontroller from 1.8V to 3.3V. The system which uses the 3.3V logic is an e-paper display and it uses SPI for communication and this is not working, so I have been trying to figure out the problem and I found out the following:
On the VCCA side, I measure 1.8V coming from the µC with no problem. It is stable. But on the VCCB side, the voltage is sometimes 3.3V and other times 1.5V. I expect it to be 3.3V as long as its input pin on VCCA side has 1.8V coming in. Or shouldn't this be the case? Also what could be the problem?
I have attached a snippet of my schematic, the part that shows the TXB0108 and its connection to the µC and Connector for the e-paper. J7 is the TXB0108, X1 is the connector for the e-paper and J1 is the µC
Any help / suggestion will be greatly appreciated. Thank you.