Other Parts Discussed in Thread: SN74AUC1G125
Hi team,
We are going to use SN74AXC1T45 to translate voltage level of the clock, from 3.3V(VCCA) to 1.1V(VCCB).
The maximum frequency of the clock is 27MHz.
Q:Is this all right? If there is any concern about this translating condition, please let me know.
In the datasheet, we couldn't find the maximum frequency(datarate) in case translating from 3.3V to 1.1V.
So we have estimated the maximum frequency from the propagation delay.
[Datasheet p10, VCCA=3.3V, VCCB=1.2±0.1V : tpd=7ns]
(Maximum frequency of the clock)=1/(2tpd)=71.4MHz
Thanks
Best Regard
Akita