Team,
I have a question regarding the SN74LVC2G07 device. Is there any chance of a continual feedback loop in the following topology? Will the signal be stuck low with no chance of being pulled high by the resistors on either side of the buffer?
Basically, I have an I2C bus that I want to isolate between two boards. Without the isolation the rise time on the bus was getting atrocious.