Other Parts Discussed in Thread: SN74AXC4T245
Hello guys,
One of my customer is about to release their new mobile product to the market.
SN74AVC4T245 is used for voltage translation of control signal between 3.3V and 1.8V in the product.
They have the following problem at this moment.
[Problem]
ICCB becomes about 2.5mA when VCCA power is not supplied.
Their condition are the followings
VCCA = 1.8V
1DIR = VCCA (through 100 kohm, 1A -> 1B direction )
2DIR = GND (through 100 kohm, 2B -> 2A direction)
1A1 = 1A2 = GND (direct to GND)
2A1 = 2A2 = open
VCCB = 3.3V
1OE = 2OE = GND (through 100 kohm)
1B1 = 1B2 = open
2B1 = 2B2 = GND (direct to GND)
They found that ICCB (VCCB consumption current) was increased to about 2.5mA when VCCA (1.8V) was powered down (open state) for sleep mode of A side.
The device datasheet says on page 6 that ICCB = 8uA (Max) with VCCA = 0V and VCCB = 0V~3.6V conditions.
The customer question is the follow.
Q. Why our ICCB is much larger (2.5mA) than datasheet spec (8uA)?
Could you please tell me how to reduce ICCB?
Your reply would be much appreciated. (Sorry. Their schematic can not be attached because they don't want to disclose their schematic)
Best regards,
Kazuya.