Replies: 2
Views: 41
Part Number: SN74AXC4T774
Hi Team,
I have two questions about this device.
1. If I have a 10 kohm pullup resistor on any of the input pins, will this device work normally?
2. Is this device suitable for open-drain applications?
Thanks.
Roy
1. Yes, if the pull-up voltage reaches VIH.
2. AXC inputs can be driven with open-drain signals (with pull-ups). AXC outputs are not open drain.
In reply to Clemens Ladisch:
Hi Clemens,
Thanks for the response! Let me check with my customer to see if they have further questions.