Replies: 1
Views: 20
Part Number: TXS0108E
Hi team,
If I have both VCCA and VCCB on the TXS0108 part set at 3.3V, can I use a 5V signal to trigger the output enable or should I voltage divide that signal down?
Thanks,
Kevin
Hi Kevin,
The info you're looking for is described in the recommended operating conditions table of the datasheet here:
As indicated above, for the OE pin, any input value above VCCA * 0.65 and less than 5.5V is considered a recommended input -- so 5V is perfectly fine.