To buffer a LVTTL signal to FPGA I am using this TI buffer SN74ALVCH16827DGGR.The buffer IC is placed on a FMC based IO card mated to a ZYNQ mother card. The problem I am facing here is when an input signal is applied to the buffer IC, there is an output signal even when there is no power supply to this IC. The output enable signals are connected to PCB GND. I want to avoid this as it may damage the FPGA. Can someone suggest me with a solution?