Hi,
I need a buffer to connect ADS803 (TI's ADC) with spartan 6 FPGA.
Could you help me choose a right buffer ?
Regards,
Karthik
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I need a buffer to connect ADS803 (TI's ADC) with spartan 6 FPGA.
Could you help me choose a right buffer ?
Regards,
Karthik
Hi Karthick
I can help you choose a buffer. Can you tell me the tipe of input signal going into the buffer and the type of output signal you need coming out. Voltage and frequency
What is Vcc,
Thanks
Hi Chris,
Thanks.
Input to Buffer :
Signal swing = Digital - CMOS level
Current = 0.5mA
Load drive capability of the input signal = 5pF (Typical)
Buffer output :
Signal swing = CMOS
Load drive capability = 10 to 20pF (It is going to be connected to Spartan 6 FPGA IOs)
Please let me know if you need any more info.
Regards,
Karthik
Hi Chris,
I am going to feed 60 3.3v cmos to FPGA IOs.
I have chosen SN74LVC2G07 buffer which seemed to suit my need.
Please confirm.
Thanks and regards,
Karthik
The 07 is open drain. If tou need open drain outputs then it should work. We also have the 6 bit version.SN74LVC07A