Hello Team,
If we use SN74AHC1G125 as a clock buffer,
Please tell us SN74AHC1G125 can use to what extent the frequency.
Best regards,
Kato
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Team,
If we use SN74AHC1G125 as a clock buffer,
Please tell us SN74AHC1G125 can use to what extent the frequency.
Best regards,
Kato
Hi Junya ,
The product folder indicates the frequency support for AHC devices to be around 75Mhz.
What is the desired frequency needed and what is the application use case? for faster freq support and faster prop delay times consider the AUC family which supports 250Mhz .
ShreyasRao said:The product folder indicates the frequency support for AHC devices to be around 75Mhz.
I think this should be listed in the datasheet as well. The product overview lists it, right.
But the nominal value of 75MHz matches the typical propagation delays given in the datasheet:
For a load capacitance of 15pF, one cycle is:
2 * 5.6ns = 11.2ns
f = 1 / 11.2ns = ~89MHz
For a load capacitance of 50pF, one cycle is:
2 * 8.1ns = 16.2ns
f = 1 / 16.2ns = ~62MHz
The difference between both is 27MHz and this halved is 13.5MHz. If you now subtract this half from 89MHz you get 75.5MHz and if you add this to 62MHz you also get 75.5MHz, so pretty close to 75MHz as nominal frequency.
Just as an information on how to estimate the operation frequency when the value is not given.
Dennis