Hi team.
My customer got a waveform as bellow.
VCC is 3.3V.
CH1:Out put
CH2:/OEpin
The output is Low when /OE voltage is 1.57V.
According to the data sheet, VIL is 0.8Vmax.
And then, the out put is High when /OE is 1.69V.
According to the data sheet, VIH is 2V min.
Why doesn't it match the data sheet value?
Sincerely.
Kengo.