This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G125-Q1: Datasheet question (over recommended spec)

Part Number: SN74LVC1G125-Q1
Other Parts Discussed in Thread: SN74LVC1G125

Hi team,

I have some questions about SN74LVC1G125-Q1.

As below image.

My question is 

1. Why do we have two Vcc condition. I mean when condition1 Vcc = 1.65V to 5.5V and the IOH = -100uA but there is also a condition2 Vcc = 1.65V and the IOH = -4mA. Does it mean we could modify the IOH and IOL?

2.What is the relationship between IOH and VOH(min)

3. If my customer need SN74LVC1G125 output fullfill VOH>3V and VOL<0.3V, how could I achieve it? (Vcc = 3.3V)

Regards,

Roy