This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] Frequently Asked Questions: Logic and Voltage Translation

Other Parts Discussed in Thread: SN74GTL2003, SN74LVC1G86, SN54BCT245, TXS0104E, SN74AC14, SN74LV1T08

Have any questions about a logic or translation device? Visit our Logic and Translation FAQ page.                                                                                                                                                        .            


Top Logic and Voltage Translation FAQs - All-Time


How does a slow or floating input affect a CMOS device?

Why does a logic device's part number have an E4/G4 suffix?

What's the difference between TTL and 5V CMOS logic?

Can the input voltage (Vi) to my logic device be higher than the supply voltage (Vcc)?

What is the difference between TXS TXB and LSF devices?

Why do the leadframes look strongly oxidized or corroded?

How do I determine the output voltage (VOH, VOL) or output current (IOH, IOL) of a CMOS logic device?

What method is best used for estimating specification values between those given in the datasheet?


Use the links below to find an answer to your question. If your question is not answered, feel free to post a question in our E2E forum. 

The "Common Applications" link will lead to our Logic Minute videos that may offer any additional help.

Common
Applications

Monostable
Multivibrators

Voltage
Translators

Input
Parameters

Output
Parameters

Power
and Thermals

Timing
Parameters

Logic
Technology

Quality and
Manufacturing

Simulation
Models