This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G125: Possible Up Level Translation Usage?

Part Number: SN74LVC1G125
Other Parts Discussed in Thread: SN74LVC1G07

Hi,

I am looking into a possible way to do up level shifting on SN74LVC1G125 with the convenience of Ioff feature. Please see the following drawing. Basically the RX data is feed into /OE and normal data input is pull to GND. When RX input is high(2.5V), CASE_RX is HiZ and pull-up by external resistor. I have done some TINA simulation where this circuitry works as expected.

Would there be any other consideration to use SN74LVC1G125 like this? Is it safe in such circuit config?

Best Regards,

Peiheng