Other Parts Discussed in Thread: TXS0104E, SN74AHC244-Q1
Hello,
Kindly review the attached design using TXS0104EQPWRQ1
Thanks,
Melbin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Kindly review the attached design using TXS0104EQPWRQ1
Thanks,
Melbin
Hello,
We are working on a project with TXS0104EQPWRQ1 in it.
Kindly review the attached schematics and let me know the review comments.
Hi Melbin,
The TXS0104E has internal 10-kΩ pull-up resistors on all I/O ports (Ax and Bx), so the external resistors R145, R150, and R151 are not typically required and I would recommend to remove them under most circumstances. If the outputs are being disabled and you need to have them held in the high state, I would recommend to increase the resistor values up to 100 kΩ. This will maintain the output voltage as high when disabled, but not cause a significant current draw during normal operation.
Otherwise the schematic looks good. I can't see the load, on either A or B port, so please take note that this device is very sensitive to heavy loads. You should maintain under 70pF at all I/O pins, and avoid long traces. Either of these can result in oscillations.
Part Number: TXS0104E-Q1
Hello,
Kindly review the attached design using TXS0104EQPWRQ1
Thanks,
Melbin
The TXS OE inputs are active high, so I would have expected pull-down resistors. Do you intend these devices to be active during power-up/-down (when the I/O states might be undefined)?
The TXS has internal pull-up resistors at the I/Os. The external pull-ups are necessary only if the B side pins are used as outputs (which is not the case if I interpret the arrows correctly).
The TXS is intended for high-speed bidirectional signals. If you have unidirectional signals that you want to translate to a lower voltage, you can simply use a buffer with overvoltage-tolerant inputs, such as the SN74AHC244-Q1.
Duplicate of TXS0104E-Q1: DESIGN REVIEW.
Hey Melbin,
As Clemens mentioned, this device isn't really necessary for unidirectional signals and you may be better suited with a buffer device like the one he suggested. Also, the pull-ups you have on the I/O will increase the Low DC offset (VIL and in turn VOL) so if that is a problem I recommend removing them if possible.
Melbin,
I noticed that you have already posted this. In an effort to consolidate posts on E2E, I have merged the threads.
Best,
Danny