Hi support team.
I received some inquiries regarding Fig 5 Icc vs frequency at P12 in datasheet from my customer.
1. Is it MHz as the unit of frequency on the horizontal axis?
2. Is the value of Icc for 1ch or the sum of all channels in Fig5?
3. Could you tell me the circuit or/and conditions as you measured?
Conditions are temperature/Load/...
My customer would like to estimate Icc on the three conditions below.
Case 1 : Using All channel is 5MHz.
Case 2 : Using 4 channels are 5MHz and other 4 channels are 10MHz
Case3 : Using 4 channels are 10MHz and other 4 channels are DC inputs.
I appreciate if you provide some information.
Let me know if you have any question.
Thank you for your cooperation.
Best regards,
Higa