Other Parts Discussed in Thread: TXS0101
I would like to have IBIS model of the MPN: TXS0104ERGYR.
I did try to use the TXS0101 IBIS, but there is just only input pin available, no output pin for simulation.
Kindly feedback on the above situation.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As I am using TXS level shifter to convert the I2C and UART signal IO voltage level of 1.8V and 3.3V, so would like to simulate the TX and RX for both direction. But there is just only input pin available so I just only can simulate one way direction which is RX at TXS switch, but unable to do TX at TXS switch.
Do you have any idea on that?