Is the IOL low-level output current of SN 74 ALS 642 A -1 NSR and SN 74 ALS 642 A -1 DW 24 mA or 48 mA?
Is this current per pin of the IC or the whole IC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is the IOL low-level output current of SN 74 ALS 642 A -1 NSR and SN 74 ALS 642 A -1 DW 24 mA or 48 mA?
Is this current per pin of the IC or the whole IC?
Hey Terao,
The datasheet lists the SN74ALS642A-1 DW package top side marking as being 'ALS642A-1'
I couldn't tell you what G624A-1 is. There isn't a device in our portfolio ending in 624A-1 so I haven't been able to track it down.
Do you believe you received the wrong device?
Thanks,
Rami