• [FAQ] Frequently Asked Questions: Logic and Voltage Translation

    Other Parts Discussed in Thread: SN74GTL2003, SN74LVC1G86, SN54BCT245, TXS0104E, SN74AC14, SN74LV1T08

    Have any questions about a logic or translation device? Visit our Logic and Translation FAQ page.                                                                                                         

  • RE: SN74LV1T126: Logic Level for OE pin

    Hi Prasenjit,

    Yes - the device can have a 5V supply and 3.3V input or 5V input -- or any combination of those. This is the primary purpose of the LV1T family of logic and is defined in the datasheet pretty clearly.

    In the Recommended Operating Conditions…

  • RE: SN74LV1T126: Logic Level for OE pin

    TI team,

    Kindly note that this query is very very urgent, as I have a fabout by next week.

  • SN74LV1T126: Logic Level for OE pin

    Part Number: SN74LV1T126

    For this part, can we connect pin A to 5V, Vcc to 5V, but drive the OE pin with 3.3V compatible logic?

    We are planning to drive OE pin from 3.3V bank of FPGA.

    Output pin we will connect it to 5V logic circuit.

     

    Please check and…

  • RE: SN74LV1T126: SN74LV1T126 have high jitter and rise time is slow

    The SN74AUC1G126 is much faster and stronger at 1.8 V. (But it does not support 3.3 V at the output.)

  • SN74LV1T126: SN74LV1T126 have high jitter and rise time is slow

    Part Number: SN74LV1T126
    Other Parts Discussed in Thread: SN74AUC1G126

    Hi, Team

    Our customer using our SN74LV1T126 as the Oscillator buffer, they using 2 pcs SN74LV1T126, one is for 3.3V, the other is 1.8V.

    the 3.3V device have no problem, but the 1.8V…

  • RE: SN74AUP1T34: Tying VCCA and A Pins

    When VCC is at GND, the B output will have high impedance. So this will work.

    A more obvious (and cheaper) solution would be to connect the data line to the OE input of the SN74LV1T126.

  • RE: SN74LV1T126: support 24.768MHz Level Shifter from 3.3V input to 1.8V output

    Where did you get that number from? At 1.8 V, max. tpd is 14 ns, which corresponds to a 35 MHz square wave.

    Anyway, for unidirectional downtranslation, you can use any buffer with overvoltage-tolerant inputs, e.g., SN74AUC1G17 with 250 MHz at 1.8 V.

  • SN74LV1T126: support 24.768MHz Level Shifter from 3.3V input to 1.8V output

    Part Number: SN74LV1T126
    Other Parts Discussed in Thread: SN74AUC1G17

    Hi, Team

    My customer needs to select a Level Shifter for the clock signal. Clock  Fsw=24.768MHz. the signal is unidirectional, and needs to transfer from 3.3V input to 1.8V output. I…

  • RE: SN74LV1T126: Level shifter understading differences between components

    Its like a serial communication, i will put a decoupling cap, thank you for your answers.

    Regards.

  • RE: SN74LV1T126: Level shifter understading differences between components

    Look OK. There should be a decoupling capacitor near each chip to prevent supply voltage dips when switching. Are you going to use PWM?

  • RE: SN74LV1T126: Level shifter understading differences between components

    Could you check if im doing right the leveling up from 3.3 to 5? please if i need resistors or cap, tell me, thank you:

  • RE: SN74LV1T126: Level shifter understading differences between components

    How many signals?

    The SN74LV1T126 does what you want. The LSF requires pull-up resistors that must be correctly sized for the desired frequency.

  • SN74LV1T126: Level shifter understading differences between components

    Part Number: SN74LV1T126

    Hi:

    I´m interested to aply a level shifter to a rgb adressable strip control, it has the next atributes and i want to understand better the component to use:

    -VCC of 5 Volts

    -Vin (data input) 0.7VCC (3.5V minimum ti have…

  • RE: SN74LV1T126: SPICE Model

    Hi Richard,

    I just want to confirm that you're using the Behavioral Spice Model from the SN74LV1T126 product folder, once you have that downloaded, please see the below FAQ. I've also went ahead and attached a test bench file with the circuit loaded in…

  • SN74LV1T126: SPICE Model

    Part Number: SN74LV1T126

    Hello,

    I need help with SN74LV1T126 SPICE Model.
    I tried to import this file in TINA, but it does not work.
    During the import process, TINA asked me to choose one of the three components:
    SN74LV1T126
    SN74LV1T126_S1
    SN74LV1T126_BUF

  • RE: SN74LV1T126: Minimum Propagation Delay

    Hi AH,

    Can you clarify on why this value is important for you? Usually only the worst case maximum propagation delay is of most importance as this will cause the most problems in a design.

    Since this device does not spec a min tpd across temperature,…

  • SN74LV1T126: Minimum Propagation Delay

    Part Number: SN74LV1T126

    Hi team,

    Can you provide data on the minimum propagation delay time for VCC = 3.3V, across temperature?

    Thanks,

    AH

  • RE: SN74LV1T126: Having 3.3V signal into this buffer w/ 1.8V power for the OE pin

    Hi,

    Yes, all inputs on this device are over-voltage tolerant which allow this device to down translate from 3.3V to 1.8V. The OE pin is an input and so it can also be powered by any voltage greater than the supply voltage up to the recommended max of…

  • SN74LV1T126: Having 3.3V signal into this buffer w/ 1.8V power for the OE pin

    Part Number: SN74LV1T126

    Our application would be required to have this buffer on the I/O sides, switching logic from 3.3V to 1.8V with 5V input tolerance. By taking a look of this buffer, it should be powered by 1.8V as below. It would be required to…

  • RE: SN74LV1T126: SN74LV1T126 vout

    The worst-case voltage drop would be 90 Ω × 2 mA = 0.18 V or 90 Ω × 4 mA = 0.36 V. (The typcial voltage drop is smaller.)

  • RE: SN74LV1T126: SN74LV1T126 vout

    Thanks you for your quick reply.

    i have a question.

    We need ICC around 2mA or 4mA.
    How many volts do you guess VOUT will be under these conditions?

    Best Regards, BANE

  • RE: SN74LV1T126: SN74LV1T126 vout

    The output transistors are MOSFETs and behave like resistors, i.e., VOH depends on the output current. The VOH specification shows that the worst-case resistance is about 90 Ω.

    What is the output current?

  • SN74LV1T126: SN74LV1T126 vout

    Part Number: SN74LV1T126

    We used IC under the following conditions.
    Why does this IC drop voltage?
    I thought I would do vCC level OUTPUT. Can you explain the mechanism?

    Input : 1.8V

    VCC :3.36V

    output:約3.12V

  • RE: SN74LV1T126: higher current alternative

    There is no other level shifter with the same pinout.

    You have to use a direction-controlled translator.