Have any questions about a logic or translation device? Visit our Logic and Translation FAQ page.
…Have any questions about a logic or translation device? Visit our Logic and Translation FAQ page.
…TXB devices cannot handle open-drain signals, as used by I²C.
For I²C, use the TXS0102 or LSF0102.
Hi Chad
Thanks for sharing the model. I was able to simulate with this. Please find attached foil with simulation result summary.
Please note that for the bus where we need the level translator, there is always a pull down (225Ohms to 650ohms) on the…
Hi Dylan
Thanks for your suggestion. I missed to add earlier that our requirement is for auto-bidirectional voltage translator. The AXC family has directional control.
I'm also checking TXB0302 if it meets our voltage level requirements. There are two…
The TXB0302/TXB0304 allow 20 kΩ resistors.
That limit is a consequence of the weak output drivers, which are necessary to allow other devices to override the voltage level, which is necessary to allow the automatic direction sensing. The TXB010x…
Due to the 1 kΩ resistors in front of the output drivers, the outputs are very weak. (This is required to allow other devices to override the voltage level.) The largest IOL that makes sense is shown in the test conditions for VOL; it is indeed…
Hello,
One of my customers has questions on the datasheet for txb0302. Can you please help comment on below items?
Kawai,
The power sequencing was modified as we had observed higher supply currents (on few devices) when one of the supply was turned off and the other was left turned on. Hence, recommend that either both supplies are ramped down together or within few…
Lidar,
The 1K series resistors are included in the IBIS model of the device.
Is the 1kohm series resistor part of the ibis model? or do i need to add it at the output of the model?
i uploaded the simulation results
Hello,
Does the component include series resistor for reducing overshoots?
When i simulate the device with its ibis model, i see high overshoot which can be resolved by adding a series resistor.
In case a resistor is part of the component…
Hi ShreyasRao,
Datasheet(ELECTRICAL CHARACTERISTICS) show IOH and IOL as test condition, but does it mean TXB0302 only provide 20 μA?
My expectation is datasheet tell me the maximum IO TXB0302 can provide without distortion. In this case DMIC module…
Hi ,
Please refer to the electrical characteristics in the datasheet (Voh and Vol) with the listed IOH and IOL current specs.
The TXB allows automatic bidirectional translation. Therefore, it has deliberately weak output drivers to allow other devices to override the voltage level.
As shown in the datasheet, its drive strength is only 20 μA.
A unidirectional translator, or a…