Other Parts Discussed in Thread: CC1121, CC1190, CC1125
Hi,
Just released the video from the range test in Cape Town with the CC1121, 868MHz, 14dBm output power, 1.2kbps and standard kit antenna.
Link: http://focus.ti.com/general/docs/video/Portal.tsp?lang=en&entryid=1_8ysxrmyk
Achieved over 25km of range with just the standard CC1121 EM reference design.
It was good fun testing the radio and getting some long range distances especially with ideal range conditions. Would be great if you achieve a greater range distance than 25km to let us know and how this was tested and configured.
Theoretically, if we included the CC1190 as well on the Tx and Rx side then we should of been able to achieve 4.75 times greater distance than the system with just CC112x. Achieved 25km with just the CC1121 so should be possible with CC112x CC1190 to achieve: 25km x 4.75 = 119km.... and this is still with a non-directional antenna :)
Please let us know if you get 25km+ distances with the CC112x family. Ideal if you can geotag the pictures and videos.
Thanks,
Richard