Other Parts Discussed in Thread: CC2531, CC2530, SIMPLICITI, CC2510, CC2511
Hi All,
IAR Systems recently released Embedded Workbench for 8051 version 7.51A. The product page at http://www.iar.com/ew8051 is now updated with information about new features, and links to Evaluation and KickStart editions of the software.
A major new feature in this release is that EW8051 now provides full support for CC2530 and CC2531. This release includes updates to the debug driver for TI LPRF SoCs, so it is now possible to debug all RF SoCs using either SmartRF04EB, SmartRF05EB and/or CC Debugger. We have also made changes to the code size limited KickStart edition in order to allow users of TIs SimpliciTI protocoll to use this edition of the tools for evaluation purposes. When used together with a development kit capable of running the SimpliciTI protocol, the code size limitation for the KickStart edition will be increased from 4kb to 16kb. All details about the new KickStart edition will soon be made available on http://www.iar.com/rfsystemonchip
* Questions & Answers
Q - Is the new kickstart version a general 16kb kickstart version for 8051 platform?
A - No. The special 16kb kickstart version of the EW8051 7.51A requires that you are developping on one of the TI RF SoC platforms capable of running SimpliciTI: CC2510-CC2511DK, CC11100-CC1111DK, CC2430DK or CC2430ZDK.
Q - What is the difference between the standard 4kb kickstart version and the extended 16kb version?
A - The two versions are both available in the kickstart distribution. The 16kb “SimpliciTI-mode” will be activated by passing the command line option ‘--ks_version’ to the linker (project->options->linker->extra options). In “SimpliciTI-mode”, the simulator will still have a 4kb code size limit, so a development kit with CC2510Fx, CC1110Fx or CC2430Fx is needed benefit from the extra code size. Our intent here is that customers buying the TI development kits should be able to fully evaluate all sample applications available in the SimpliciTI distribution.
Thanks for reading!
/Henrik