This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unexpected responding from CC3000

I'm porting CC3000 (mRata LBWA1ZZVK7 rev2.0) to ST MCU (with STM32F4 discovery board). I can send command and receiving IRQ interrupt, but problem is feeback from CC3000 is wrong.

I have debugged and saw what had happened in function SimpleLink_Init_Start()  as below:

HOST -> CC3000: 01 00 05 00 00 01 00 40 01 00

CC3000 -> HOST: 02 00 FF 00 00 00 00 00 00 00 (same result in example -> SPI is good)

Got IRQ interrupt (go low):

HOST -> CC3000: 03 00 00 00 ...

CC3000 -> HOST: 02 04 04 04 ... -> wreid result, except right opcode feedback 02 for 03, all fb bytes are 04

I tried with function nvmem_read_sp_version() but still got above problem.