Hi,
Quick question, SpiResumeSpi() is expected to be in the spi.c file (but SpiPauseSpi() isn't), and from the example I am looking at, it simply disables the IRQ interrupt which comes from the CC3000 to the host.
Could I ask why the the CC3000HostDriver doesn't use use the registered tWlanInterruptEnable type function pointer registered with wlan_init? They both seem to achieve the same thing.
I haven't spent much time in the HostDriver code, as I'm focused on spi.c, but is there a potential different use case for this function that I don't know about besides enable interrupts on IRQ from CC3000? such as is there a reason why the IRQ pin interrupt wouldn't be disabled?
Cheers
EDIT: See here for a response. http://e2e.ti.com/support/low_power_rf/f/851/t/306593.aspx