This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi E2E,
What is the part number of the JTAG header present on the LAUNCHXL2-570LC43 launchpad?
Regards,
Carlo
Hi Carlo,
The JTAG header on launchpad is cTI20.
cTI 20-pin Header Information
The header features 2 rows of 10 pins each, 0.05" (1.27mm) pin pitch, 0.10" (2.54mm) row pitch. Pin 6 is keyed.
IMPORTANT! The part numbers below are based on the manufacturers' specifications, which can change without prior notice.
Manufacturer: Samtec
Manufacturer: OUPIIN
Manufacturer: Don Connex