Part Number: SAFETI_DIAG_LIB
I am running demo app for the SafeTI diagnostics library (2.4.0) for the Hercules TMS570LC4357 on a TMDX570LC43HDK development kit.
In the TMS570LC4357_NoOS file HL_sys_startup.c the function call resetReason = SL_Init_ResetReason(); returns a number of values.
Two of the values returned are:
RESET_TYPE_CPU1 = 10u,
RESET_TYPE_ICSTRST = 11u
These are defined in sl_types.h.
As part of the installation of the SafeTI diagnostics library there is SafeTIDiagnosticLibrary-User'sGuide-v2.4.0.chm.
However, this user guide does not document what causes RESET_TYPE_CPU1 and RESET_TYPE_ICSTRST.
Is there a more up to date version of the user's guide that includes this information?
Also, what is the difference between RESET_TYPE_EXTRST and RESET_TYPE_EXTRST_NERROR?