Part Number: RM46L850
Other Parts Discussed in Thread: HALCOGEN, TMS570LC4357, , LAUNCHXL2-RM46
I'm using HALCoGen generated startup code and linker file. I'm using gcc format outputs.
In C++, if I have a class which is instantiated global, the constructor is never called.
static myClass myClassObj;
I was never hitting a breakpoint in the constructor, nor were the member variables being set.
I used some code outlined here in the section Coverage Constructors.
https://mcuoneclipse.com/2014/12/26/code-coverage-for-embedded-target-with-eclipse-gcc-and-gcov/
The linker file already outputted the .init_array all that was needed was the execution of this function.
/* call the coverage initializers if not done by startup code */void static_init(void) { void (**p)(void); extern uint32_t __init_array_start, __init_array_end; /* linker defined symbols, array of function pointers */ uint32_t beg = (uint32_t)&__init_array_start; uint32_t end = (uint32_t)&__init_array_end; while(beg<end) { p = (void(**)(void))beg; /* get function pointer */ (*p)(); /* call constructor */ beg += sizeof(p); /* next pointer */ }}Is the constructor execution supposed to happen automatically in TI code? In the past I've used HALCoGen and I don't recall needing to do this.