When I load a binary image for flashing in the Uniflash GUI, it correctly detects that the file is binary (rather than ELF):
When I try to use the same file with the command line (dslite.bat), I get an error saying "Could not determine target type of file".
Is there a setting I can use to make the command line version understand that the input file is a binary file?