Part Number: DK-TM4C129X
i am working on kentech display with dk-tm4c129x board
i am plot a image on display its successfully print.
now i want to how image color put on screen
in below index color of image how it put on screen
GrImageDraw(&sContext, g_pui8LightOn,0,0);
* red backgraound is color of index
//*****************************************************************************
//
// This is the image of a red LED that is turned on.
//
//*****************************************************************************
const uint8_t g_pui8LightOn[] =
{
IMAGE_FMT_4BPP_COMP,
20, 0,
20, 0,
15,
0x00, 0x00, 0x00,
0x00, 0x00, 0x16,
0x00, 0x00, 0x40,
0x00, 0x00, 0x76,
0x00, 0x00, 0x9b,
0x00, 0x00, 0xac,
0x00, 0x00, 0xb6,
0x00, 0x00, 0xbc,
0x00, 0x00, 0xbe,
0x00, 0x00, 0xbf,
0x00, 0x00, 0xc1,
0x00, 0x00, 0xc5,
0x00, 0x00, 0xcd,
0x00, 0x00, 0xdb,
0x00, 0x00, 0xef,
0x00, 0x00, 0xfc,
0x84, 0x01, 0x13, 0xaf, 0xe7, 0x31, 0x03, 0x1b, 0xff, 0x09, 0xff, 0xee,
0xee, 0x51, 0x01, 0x02, 0xff, 0xb1, 0x02, 0xdd, 0xcc, 0x20, 0x00, 0x00,
0x2f, 0xbb, 0xcc, 0x10, 0x92, 0x00, 0x01, 0x72, 0xdc, 0xcc, 0xcb, 0x96,
0x00, 0x10, 0x07, 0xff, 0xfe, 0xed, 0xdc, 0xcc, 0xbb, 0x08, 0xba, 0x96,
0x30, 0x1e, 0x22, 0xba, 0xaa, 0xaa, 0x10, 0x86, 0x51, 0x3e, 0x69, 0xba,
0x99, 0x99, 0x99, 0x01, 0x76, 0x52, 0x5d, 0xee, 0xdd, 0xcb, 0xa9, 0xb2,
0x20, 0x53, 0xcd, 0x6c, 0x98, 0x76, 0x54, 0xcc, 0xdd, 0x40, 0xcc, 0x6a,
0x97, 0x66, 0x43, 0x5c, 0xcc, 0xba, 0x40, 0x98, 0x19, 0x87, 0x65, 0x43,
0x3c, 0xcb, 0xa9, 0x20, 0x98, 0x89, 0x1a, 0x42, 0x1a, 0x88, 0x98, 0x77,
0x40, 0x88, 0x69, 0x44, 0x31, 0x04, 0x67, 0x77, 0x77, 0x00, 0x78, 0x88,
0x76, 0x55, 0x44, 0x20, 0x01, 0x55, 0x00, 0x66, 0x66, 0x77, 0x77, 0x65,
0x54, 0x43, 0x10, 0x00, 0x00, 0x24, 0x55, 0x55, 0x66, 0x65, 0x54, 0x44,
0x00, 0x31, 0x00, 0x00, 0x02, 0x44, 0x45, 0x55, 0x54, 0x00, 0x44, 0x33,
0x10, 0x00, 0x00, 0x00, 0x13, 0x44, 0x08, 0x44, 0x44, 0x33, 0x21, 0xb9,
0x00, 0x00, 0x12, 0x10, 0x33, 0x32, 0x20, 0xba,
};