Part Number: MSP-EXP432P401R
Hi,
I am using a function called ADCBuf_convert() to capture values.
One thing I would like is to capture the data as single-ended rather than differential. I have tried the function ADC14_setResultFormat(ADC_UNSIGNED_BINARY) to set the ADC14DF to 0. However, during the call to ADCBuf_convert() the format gets changed back to ADC14DF to 1. I cannot see where this gets changed back.
Can you suggest a setup/process to set the ADC14DF value to ADC_UNSIGNED_BINARY for this call? Is there an alternative function call that can be used?
Malcolm