In Our design QSPI interface was required to communicate to the LAN9253,
In RM48L952PGE_144 pin MCU has only single SPI feature only.
Is there any way to make QSPI interface with RM48L952PGE_144 .
Thanks and Regards,
Ganesh V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In Our design QSPI interface was required to communicate to the LAN9253,
In RM48L952PGE_144 pin MCU has only single SPI feature only.
Is there any way to make QSPI interface with RM48L952PGE_144 .
Thanks and Regards,
Ganesh V
Hi Ganesh,
RM48Lx and TMS570 don't support QSPI, but they support multi-buffered SPI in parallel mode (MibSPI in parallel). MibSPI in parallel is full-duplex communication, but QSPI is half-duplex.
The communication protocols are also different:
1. QSPI: The following waveform is for charlen = 8-bit
As you can see 4 bits are transferred every clock cycle. The bit order is QIO0 sends bit4, QIO1 sends bit5 and so on in the first clock cycle and bits 0,1,3, and 3 are sent out in the 2nd clock cycle.
2. MibSPI in parallel: The following waveform is for charlen=16-bit
In 4-data line mode (master mode) the shift register bits 15, 11, 7, and 3 will be connected to the pins SIMO[3], SIMO[2], SIMO[1], and SIMO[0], and the shift register bits 12, 8, 4, and 0 will be connected to the pins SOMI[3], SOMI[2], SOMI[1], and SOMI[0]. The subsequent rising edge of SPICLK will shift data in the shift register by 1 bit to the left (SIMO[3] will shift the data out from bit 15 to 12, SIMO[2] will shift the data out from bit 11 to 8, SIMO[1] will shift the data out from bit 7 to 4, SIMO[0] will shift the data out from bit 3 to 0). After four SPICLK cycles, when the full data word is transferred, the shift register (16 bits) is copied to the receive buffer, and the RXINT flag will be set.