This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM48L952: We are Using Specturm Digital XDS560V2 STM USB Emulator with our Custom Board with ETM Interface to RM48L952 I get the error Problem of Trace Analyzer on Cortex R4

Part Number: RM48L952


Hi ,

We are Using Specturm Digital XDS560V2 STM USB Emulator with our Custom Board with ETM Interface to RM48L952 I get the error Problem of Trace Analyzer on Cortex R4

I am Enabling Trace and as Shown in the attached Image I get the following error

We are not understanding What is the root cause for this error .

Could not run analyzer on Cortex R4. Cause:

Read device ID did not match the device descriptions available.

Possible reasons:

(1) Target is not connected

(2) Trace support for the device is not available in the version of the software.

Error Displayed

Connectivity Test in Code Composer Studio

Specturm Digital XDS560V2 STM USB Emulator  Connectivity in Command Prompt