This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS0432: TMS570LS0432

Part Number: TMS570LS0432
Other Parts Discussed in Thread: BQ76PL455EVM,

Hi,

I am trying to program the TMS570432 Launchpad with the sample code provided by TI to work with the BQ76PL455EVM.

I see the "NOTE: Make sure that the resistor R8 is removed on the TMS570 Launchpad board."

 It's that mean R8 resistors need to be heat and remove with a soldering iron?

I have a question : I found that the circuit diagram R8 in the design document is 0 ohm. After removing it, the circuit is open, right?

If  circuit is open the pin38  SCI1_RX can work normal to receive BQ76PL455EVM data?