Other Parts Discussed in Thread: BQ76PL455EVM,
Hi,
I am trying to program the TMS570432 Launchpad with the sample code provided by TI to work with the BQ76PL455EVM.
I see the "NOTE: Make sure that the resistor R8 is removed on the TMS570 Launchpad board."

It's that mean R8 resistors need to be heat and remove with a soldering iron?
I have a question : I found that the circuit diagram R8 in the design document is 0 ohm. After removing it, the circuit is open, right?
If circuit is open the pin38 SCI1_RX can work normal to receive BQ76PL455EVM data?