Part Number: MSP432E411Y
I'm using an MSP432P411V, not the E part. To reduce power consumption, I want to run the CPU at a rate slower than the default 48MHz - perhaps 24 MHz or even 14MHz. How do I do this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432E411Y
I'm using an MSP432P411V, not the E part. To reduce power consumption, I want to run the CPU at a rate slower than the default 48MHz - perhaps 24 MHz or even 14MHz. How do I do this?
As far as I know, the P411x series (like the P401R) start up with MCLK=DCO=3MHz (DCORSEL=1).
I needed to change initialPerfLevel
PowerMSP432_PerfLevel myPerfLevels[] =
{
{
.activeState = PCM_AM_DCDC_VCORE0,
.VCORE = 0,
.clockSource = CS_DCOCLK_SELECT,
.DCORESEL = CS_DCO_TUNE_FREQ,
.tuneFreqDCO = 8000000,
.SELM = CS_DCOCLK_SELECT,
.DIVM = CS_CLOCK_DIVIDER_1,
.SELS = CS_DCOCLK_SELECT,
.DIVHS = CS_CLOCK_DIVIDER_1,
.DIVS = CS_CLOCK_DIVIDER_1,
.SELB = CS_REFOCLK_SELECT,
.SELA = CS_REFOCLK_SELECT,
.DIVA = CS_CLOCK_DIVIDER_1,
.flashWaitStates = 0,
.enableFlashBuffer = true,
.MCLK = 8000000,
.HSMCLK = 8000000,
.SMCLK = 8000000,
.BCLK = 32768,
.ACLK = 32768,
}
};
#if 1
const PowerMSP432_ConfigV1 PowerMSP432_config = {
.policyInitFxn = &PowerMSP432_initPolicy,
.policyFxn = &PowerMSP432_deepSleepPolicy,
.initialPerfLevel = 4,
.enablePolicy = true,
.enablePerf = true,
.enableParking = true,
.customPerfLevels = myPerfLevels,
.numCustom = sizeof(myPerfLevels) / sizeof(PowerMSP432_PerfLevel),
.useExtendedPerf = true,
.enableInterruptsCS = true,
.priorityInterruptsCS = ~0,
.isrCS = 0,
};
#else
const PowerMSP432_ConfigV1 PowerMSP432_config =
{
.policyInitFxn = &PowerMSP432_initPolicy,
.policyFxn = &PowerMSP432_deepSleepPolicy,
.initialPerfLevel = 0,
.enablePolicy = true,
.enablePerf = true,
.enableParking = true
};
#endif