Part Number: TM4C123BH6ZRB
Hey,
we use TM4C123BH6ZRB bootloader to flash the TIVA via SPI.
On SPI master (i.MX 6) which downloads the binary file I have to set the block transfer size (must be a multiple of four).
Now I'm wondering about different max. block sizes: on device accepts 240 bytes, others max. 60 bytes.
Is there a legacy limit on older ROM functions (firmware)?
Best regards,
Tobi