I am attempting to connect to a new target PCBA using the ICDI debugger tool to an unprogrammed device and getting the error: CORTEX_M4_0: Error connecting to the target.
I have checked the following:
VDD,VDDA,VDDAREF,VDDC power supply signal levels normal.
Oscillator signal levels normal.
Reset signal normal
ICDI connects to a nearly identical target using TM4C123AH6PMI device with same oscillator without issue.
JTAG signals when connecting to target device:
TCLK active
TMS low
TDI data packet transmitted
TDO remains logic high.
Reset remains logic high (2.8V)
Any suggestions of additional items to check or try?