This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DK-TM4C129X: Alternative evaluation module to DK-TM4C129X

Part Number: DK-TM4C129X

Hi Team,

Our customer is using the DK-TM4C129X to upgrade the firmware of TM4C1297NCZAD13 as shown in the pictures below.

  

I understand from the E2E thread below that there are no plans to rebuild the the DK-TM4C129X.

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1095072/dk-tm4c129x-tivaware-development-kit-lifecycle-question

Our customer is considering similar low cost evaluation board with In-Circuit Debug Interface (ICDI) such as EK-TM4C1294XL Launchpad to load the firmware to TM4C1297NCZAD13. However, the 10-pin connector in EK-TM4C1294XL is 2x5 whereas in DK-TM4C129X it's 1x10. It seems that the customer have to build their own cable to fit their existing board and the ICDI of EK-TM4C1294XL Launchpad. Can you please confirm if the EK-TM4C1294XL Launchpad can program TM4C1297NCZAD13?

Regards,

Danilo