The datasheet writes ...
"In the Terminal Functions table below, the "Reset Pull State" is the state of the pull applied to the terminal while nPORRST is low and immediately after nPORRST goes High. The default pull direction may change when software configures the pin for an alternate function. The "Pull Type" is the type of pull asserted when the signal name in bold is enabled for the given terminal by the IOMM control registers."
What happens to the PU/PDs between "immediately after nPORRST" and to when the software configures the ports?
I want to make sure the PU/PW are active until sw configures them.